BQT6904400-03

Unpacking Cubicles

NOTICE
HAZARD OF inappropriate handling
To avoid any damage to the front cubicle components of the functional unit, keep the protection foam in place until the switchboard is in the operation phase.
Failure to follow these instructions can result in equipment damage.
NOTE: The preparation of cubicles must be carried out only on the premises where they will be installed.

Follow the below steps to unpack the cubicle:

  1. Unpack the functional unit by removing the wooden columns (3), then the plastic cover (2).

  2. Remove the cubicle packaging.

  3. Remove the lifting brackets (1).

Figure 11
Unpacking of Cubicle

1

Lifting brackets

2

Plastic cover

3

Wooden columns

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?