BQT6904400-03

Rack-In Check

NOTE: Each time a cubicle is linked to another one, check that the mobile part can be racked-in and locked in position properly.

For the insertion and racking-in of the mobile part and to open the door, refer to Operations, User Guide (BQT6904800).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?