BQT6904400-03

Cable Termination Height

Figure 73
Cable Termination Height

NOTE: If required, cable termination height can be increased by adding a cable box below the bottom sheet. For details, contact Schneider Electric.

Table 16 Cable Termination Height

Rated voltage (kV)

Type of cubicle

Configuration

H (mm)

7.2/12

I/F (400 mm)

315 A

400

12/17.5

I/F (650 mm)

630 A

680

1250 A

680

I/F (800 mm)

1250 A

550

2000 A

550

I/F (1000 mm)

2500 A

550

3150 A

450

4000 A

450

24

I/F (800 mm)

630 A

650

800 A

650

I/F (1000 mm)

1250 A

650

2000 A

650

2500 A

650

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?