Fastening of the Cubicles
WARNING |
|---|
|
hazard of installing under inadequate conditions
Do not allow a cubicle to be raised after the next one
is installed to avoid vibrations caused by load.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
| NOTICE |
|---|
|
hazard of installing under inadequate conditions
Failure to follow these instructions can result in equipment damage.
|
| NOTICE |
|---|
|
hazard of inappropriate assembly
Comply with precise measurements for the placement of
the cubicle, as the positioning of the first cubicle determines the
placement of the remaining cubicles.
Failure to follow these instructions can result in equipment damage.
|
Fastening on Concrete Foundations
Follow the below steps to fasten the cubicle to the floor on standard civil engineering works:
-
Position first cubicle on the floor in accordance with the switchgear-specific space assignment plan, refer to Ground Plan of a MCSeT Switchgear within a Switchgear Room
. -
Remove the cable compartment cover. Refer to Access to the Cable Compartments, User Guide (BQT6904800).
-
Once the cubicle is positioned:
-
Verify that the cubicle front is correctly aligned both horizontally and vertically.
-
If necessary, raise the cubicle and insert shims below the cubicle near the fastening points until the correct horizontal position is achieved, refer to Figure 27
.
-
-
Fasten the cubicle with screws to the two fastening points on both the front end and the rear end.
Figure 27
Cubicle Fastening on Concrete
Foundations
|
1 |
Screw M10 x 30 |
4 |
Shim plate(1) |
|
2 |
Spring lock washer M10 |
5 |
Slotted set screw M10 x 30 |
|
3 |
Plain washer |
6 |
Plate 3 mm |
|
(1) Add shim plates as needed. |
|||
Additional Fastening Variants (C-Channel)
The additional fastening variants are available on request. For details, contact the manufacturer.
Follow the below steps to fasten the cubicle on C-channel rails on standard civil engineering works:
-
Drill holes into the C-channel frames at the intended cubicle fastening points, refer to Figure 28.
-
Position the cubicle on the C-channel rails, aligning the fastening points.
-
Insert dowel pin and other suitable fasteners (provided by Schneider Electric) refer to Figure 29.
-
Securely fasten the cubicle to the C-channel rails at the designated points.
-
The additional fastening variants are available on request. For details, contact Schneider Electric.
-
C-channel rails are not be provided by Schneider Electric.
Figure 28
Dimension
of the Floor Space and C-Channel Rails
| Rated voltage (kV) |
Dimensions (mm) |
||
|---|---|---|---|
|
A |
B |
C |
|
|
7.2/12/17.5 |
1340 |
1290 |
1240 |
|
24 |
1800 |
1750 |
1700 |
Figure 29
Cubicle Fastening on Base
Frame
|
1 |
Allen screw M12 x 45 |
4 |
Dowel pin |
|
2 |
Washer M12 |
5 |
C-channel rail |
|
3 |
Square washer |
WARNING