BQT6904400-04

Requirements of the Switchgear Room

CAUTION
hazard of incorrect dimensions
Adhere to the specified spacing dimensions around the switchboard, refer to Table 15.
Failure to follow these instructions can result in injury or equipment damage.

Prior to the installation of switchgear cubicles, refer to Civil Engineering Guide (BQT8706400) and make sure that the switchgear room complies with the below requirements:

  • Observe the minimum distance between the switchgear and the wall of the room.

  • The load-bearing capacity of the fastening areas must correspond to the weight of the switchgear (perform a stress analysis of the building).

  • Check base frame (if used) for dimensions and positional tolerances.

  • Check position of floor openings for MV and LV cables.

NOTE: Observe switchgear-specific space assignment plan, refer to Ground Plan of a MCSeT Switchgear within a Switchgear Room.

Table 15 Pressure Relief Exhausts and Civil Engineering Utility Space

Pressure relief

Switchboard external exhaust

Switchboard internal exhaust

Tunnel

Tunnel and absorber

Rated voltage (kV)

Basic structure panel dimension (mm)

Pressure relief

Outside the building tunnel
dimension (mm)

Inside the building tunnel and absorber
dimension (mm)

Ur

H

LV

H1(2)

T(3)

H2

H3(4)

H1(2)

T(3)

A

H2

H3

Up to 12/17.5

2240

580

2710

470

3000

200

2710

470

260

3400

680

24

2400

630

2950

550

3150

200

2850

450

220

3500

650

(1) R - Distance to rear wall, 200 mm (AFL) and minimum 800 mm (AFLR).

(2) With standard LV cabinet 630 mm. Increased height of LV cabinet is available, without impact on the ceiling height.

(3) Height of the tunnel is inclusive of flange (40 mm for 24 kV and 12/17.5 kV).

(4) Minimum 200 mm.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.