BQT6904400-03

Preparation

WARNING
hazard of incorrect operation
Ensure the assembly instructions for the test adapters and the operating and inspection instructions for the test unit.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Isolate I/F cable of the cubicle to be tested.

  2. Isolate I/F cable in remote station.

  3. Earth I/F cable of the cubicle to be tested.

  4. Remove cable compartment cover. Refer to Access to the Cable Compartment, User Guide (BQT6904800).

  5. Disconnect VT and surge arrester.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?