BQT6904400-03

Transport with Forklift Truck

WARNING
HAZARD OF toppling
  • When transporting the switchgear, ensure that the units do not tilt or tip.
  • Nail down transport pallets to the loading surface.
  • For transporting the trucks, comply with the transport specifications in the appropriate manuals.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
HAZARD of Equipment toppling
  • For transport, the cubicles must be packaged completely.
  • The entire length of the forks must be placed under the transport unit.
Failure to follow these instructions can result in injury or equipment damage.

Figure 10
Transport with Forklift Truck

Delivery

Shipping units must be checked upon receipt. Any damage which may have occurred in transit must be recorded and reported to the manufacturer immediately.

NOTICE
HAZARD OF incorrect HANDLING
  • Competent operators must handle the lifting of the cubicle.
  • It is recommended to use inspected cranes or forklifts for transportation.
  • The lifting or handling of the cubicle from the loaded transportation vehicle should be done safely.
  • Careful disassembly of the packaging is essential to help prevent damage to the cubicle.
Failure to follow these instructions can result in equipment damage.
NOTE:
  • Check completeness of consignment based on the transport documents.

  • The supplier must be notified in writing without delay about any deviations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?