Installing the End Cover
DANGER |
|---|
|
HAZARD OF electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
Follow the below steps to install the end cover:
-
Install the busbar end cover (1) with rivet screw (2).
-
Install the front end cover (8) and rear end cover (3), and install the bolts (7) along with washers (6) (Figure 111). Apply the torque as per ST0171.
-
Install the center end wall coupler (4) and tunnel end wall coupler (5) with hardware.
-
Remove the cover plate from the knock-out (9) at the left end of the cubicle (Figure 111), and feed the earth bus rod into the knock-out hole (one per cubicle).
Figure 111
Installing the End Covers (Sheet
1 of 2)
Figure 111
Installing the End Covers (Sheet
2 of 2)
|
1 |
Busbar end cover |
6 |
Washer M8 |
|
2 |
Rivet screw |
7 |
Screw M8 x 25 |
|
3 |
Rear end cover |
8 |
Front end cover |
|
4 |
Center end wall coupler |
9 |
Knock-out |
|
5 |
Tunnel end wall coupler |
DANGER