BQT6904400-03

General Information

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • Only qualified personnel must perform cable terminations and cable installation.
  • Make sure that the cable dielectric insulation does not contact any grounded metal parts or other phases.
  • The grounded metallic support must be in contact with the external protective cable sheath.
Failure to follow these instructions will result in death or serious injury.

This section provides information for all types of cables.

Retrieve: The floor plates, cable support and hardware bag from the cubicle packaging.

To access the interior of a cubicle. Refer to Access to the Main Circuit Compartments, User Guide (BQT6904800).

Figure 64
3 Single-Pole Cables

Figure 65
1 Three-Pole Cable

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?