BQT6904400-04

Installing the Current Transformers

Follow the below steps to assemble the CT:

  1. Place the CT (2) on the mounting plate (1) (Figure 80).

  2. Insert the washers (4) and the screws (3) in the mounting holes at each corner of the CT (2).

  3. Tighten each screw (3) to a torque of 68 N•m.


Installing P1 Connections:
  1. Place the spout to CT connection (7) in position.

  2. Insert the washers (6) and the screws (5).

  3. Tighten each screw (5) to a torque of 68 N•m.


Installing P2 Connections:
  1. Place the E/S to CT connection (8) in position.

  2. Insert the washers (6) and the screws (5).

  3. Tighten each screw (5) to a torque of 68 N•m.

  4. Place the cables connection (9) in correct position to the E/S to CT connection (8).

  5. Install the screws (10) along with the washers (11) and the nuts (12).

  6. Tighten each nuts (12) to a torque of 68 N•m.

  7. Install the sensor TH110 (13) on the E/S to CT connection (8).

Figure 80
Installing the Current Transformers

1

Mounting plate

8

E/S to CT connection

2

CT

9

Cable connection

3

Screw M12 x 35

10

Screw M12 x 40

4

Washer M12

11

Washer M12

5

Screw M12 x 45

12

Nut M12

6

Washer M12

13

TH110 sensor

7

Spout to CT connection

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.