BQT6904400-04

About the Document

Document Scope

This installation guide describes about air-insulated MV switchgear units of the MCSeT.

  • This guide is meant for qualified person who will install MCSeT equipment: panel builder, installer or end user.

  • This installation guide cannot be used to define or check the devices compatibility with every single users application, nor its reliability within it. It is the duty of every user or panel builder to perform a complete risk analysis, evaluation and testing of the products in specific applications in accordance with applicable standards.

  • In order to help ensure the right functioning of the device installed in the equipment, refer to the equipment manufacturer documentation.

  • When the products are used in applications with specific technical and safety rules, must follow the integration and protection rules for the specific application.

All dimensions not specified in detail are in millimeters.

Validity Note

This guide is valid only for MCSeT cubicle. The design provides easy rack-in/rack-out operation without the need for a separate trolley. This MCSeT cubicle is an extension of the MCSeT range and delivers performances up to 24 kV, equipped with EvoPacT HVX VCB and CVX Contactor. It also has other functional trolley like the EvoPacT Metering Truck (MTX).

For product compliance and environmental information (RoHS, REACH, PEP, EOLI, and so on), go to the Green Premium page on the Schneider Electric website.

The information contained in this guide is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on https://www.se.com/ww/en/download.

The technical characteristics of the devices described in this guide also appear online. To access the information online, go to the Schneider Electric home page at www.se.com.

Product Related Information

Air-insulated MV switchgear units of the MCSeT series are designed exclusively for switching and distributing electrical power.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The MCSeT switchgear must be used only in scope of specified standards and specific technical data.
Failure to follow these instructions will result in death or serious injury.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Related Documents

The following additional documents must be complied with:

  • Purchase agreement with the stipulations regarding the switchgear-specific equipment and the legal details.

  • The appropriate switchgear-specific circuit diagrams/documentation.

  • The operating manuals of the LV devices installed in the switchgear (for example, voltage presence detecting systems and devices in LV cabinet).

  • The assembly drawings supplied with the equipment.

  • The assembly instructions of the manufacturer of the cable connection systems to be connected to the switchgear.

  • The operating instructions of the trucks being used.

Title of Document

Reference Number

EvoPacT HVX Catalog 2024 (IEC)

NRJCAT21051EN-IEC

User and Maintenance Guide

BQT6904800-00

Civil Engineering Guide

BQT8706400-00

Receipt Guide

BQT8677900-00

To find documents online, visit the Schneider Electric download center (www.se.com/ww/en/download/).

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Queries

For any questions, suggestions, or need of further information about this guide, contact Schneider Electric. For additional details, visit our website www.se.com.

For details of MCSeT switchgear expansion (either right or left side), it is recommended to contact Schneider Electric.

We always strive to provide you with the best-possible information for optimum, safe use of our products. Contact Schneider Electric if you have any recommendations, amendments, or proposals for improvement.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.