NHA2779002-12

Alarms counters

Every occurrence of each type of alarm is counted and recorded in the meter.

Alarms rollover value

The alarm counters roll over to zero after reaching the value 9999.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.