NHA2779002-12

Panel Meter

The back of your meter supports various power system connections.
A Auxiliary power supply (control power) terminals (L+, L-)
B Input voltage terminals (V1, V2, V3, VN)
C Optional I/O Slot (Only for PM2130)
D Input current terminals (I1+, I1-, I2+, I2-, I3+, I3-)
E RS-485 communications (D0, D1, SHLD, 0V) / POP terminals (D1+, D1-)
F Gasket
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.