NHA2779002-12

Thermal demand

Thermal demand calculates the demand based on a thermal response, which imitates the function of thermal demand meters.

The demand calculation updates at the end of each interval. You can set the demand interval from 1 to 60 minutes (in 1-minute increments).

Thermal demand example

The following illustration shows the thermal demand calculation. In this example, the interval is set to 15 minutes. The interval is a window of time that moves across the timeline. The calculation updates at the end of each interval.

The image illustrates how thermal demand is calculated over time using a moving 15-minute interval. The x-axis represents time in minutes, segmented into consecutive 15-minute intervals. The y-axis indicates the percentage of load, with values such as 99% and 90% shown. The calculation updates at the end of each interval, with the demand value based on the last completed interval.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.