NHA2779002-12

Digital output applications

The meter is equipped with two digital output ports (D1, D2). You can configure the digital outputs for use in the following applications:

Switching applications, for example, to provide on/off control signals for switching capacitor banks, generators, and other external devices and equipment.

Energy pulsing applications, where a receiving device determines energy usage by counting the kWh pulses coming from the meter’s digital output port.

Unary, digital and standard alarm configurations.

Wiring the digital output

Default digital output state

The default digital output state for I/O pin is high (switch closed). The digital output state for I/O pin can be changed through communication.

I/O pin state

External mode

Alarm

Display

Comm

Switch

Low

0

0

OFF

0

Open

0

1

ON

1

Closed

0

0

OFF

0

Open

1

0

ON

1

Closed

High

0

0

OFF

0

Closed

0

1

ON

1

Open

0

0

OFF

0

Closed

1

0

ON

1

Open

Demand parameter for digital output

The associating demand parameters (Present demand (VA, W, VAR), Last demand (VA, W, VAR) and Predict demand (VA, W, VAR)) can be configured for digital output based on alarm events when exceeds the set upper limit. Only one demand parameter can be set at a given time.

NOTE: The alarm set up is done through communication using ION setup.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.