NHA2779002-12

Setup screen menus

Setup screen enables you to configure various setup parameters.

Below is the list of setup parameters and the configurations it supports.

Meter setup menus

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.