NHA2779002-12

China Standard Compliance

This product complies with the following standards in China:

PM2110 / PM2120

BS/EN/IEC/UL* 61010-1 Safety requirements for electrical equipment for measurement, control, and laboratory use - Part 1: General requirements

PM2130

BS/EN/IEC 61557-12 Electrical safety in low voltage distribution systems up to 1 000 V AC and 1 500 V DC - Equipment for testing, measuring or monitoring of protective measures - Part 12: Power metering and monitoring devices (PMD)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.