NHA2779002-12

Energy measurements

The meter provides fully bi-directional, 4-quadrant energy metering.

The meter stores all accumulated active, reactive and apparent energy measurements in nonvolatile memory:

  • kWh, kVARh, kVAh (delivered)

  • kWh, kVARh, kVAh (received)

  • kWh, kVARh, kVAh net (delivered - received)

  • kWh, kVARh, kVAh absolute (delivered + received)

All energy parameters represent the total for all three phases.

NOTE: Based on the energy scale selection, when kWh, kVARh, kVAh (delivered) or kWh, kVARh, kVAh (received) of the energy parameters overflow at 999999999.999 all energy parameters value resets.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.