NHA2779002-12

Viewing demand values in Setup screen

The meter supports editing power and current demand through setup mode.
  1. Press and hold the Up and Down buttons simultaneously for 2 seconds to enter Setup.
  2. Enter password. Default password is 0000.
  3. Press OK.
  4. Press the Down button to select Pd (power demand) or Ad (current demand) parameter.
  5. Press OK.
  6. Press the Down button to select required values from the existing list.
  7. Press OK.
  8. Press and hold the Up and Down buttons simultaneously for 2 seconds to exit Setup.
  9. Select Yes to save your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.