NHA2779002-12

Heartbeat/serial communications LED

The heartbeat/serial communications LED blinks to indicate the meter’s operation and serial Modbus communication status.

The LED blinks at a slow, steady rate to indicate the meter is operational. The LED flashes at a variable, faster rate when the meter is communicating over a Modbus serial communications port.

NOTE:
  • You cannot configure this LED for other purposes.

  • If the LED remains lit without blinking or flashing, it may indicate a technical problem. In this case, power down the meter and reapply power. If the problem persists, contact Technical Support.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.