NHA2779002-12

Setting up the password

The meter password can only be configured through the front panel.

The factory-default setting for all passwords is “0000” (zero). Changing the default password for screens that are password protected prevents unauthorized personnel from accessing certain screens such as the Setup and Clear screens.

To change the meter password using Setup, follow these steps:

  1. Press and hold the Up and Down buttons simultaneously for 2 seconds to enter Setup.

  2. Enter password. Default password is 0000.

  3. Press OK.

  4. Press the Down button to select PASS (password) parameter.

  5. Press OK.

  6. Press the Down button to change the digits.

    NOTE: Hold Down button for 2 seconds to move the cursor to the next digit.
  7. Press OK.

  8. Press and hold the Up and Down buttons simultaneously for 2 seconds to exit Setup.

  9. Select Yes to save your settings.

Password settings

Parameter Values Description
Pass 0000 - 9999 Sets the password for accessing the meter setup screen.
NOTE: Common password applies across all parameters.

Lost password

Visit www.se.com for support and assistance with lost passwords or other technical problems with the meter. Make sure you include your meter’s model, serial number and firmware version in your email or have it readily available if calling Technical Support.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.