NHA2779002-12

Clear parameters

The meter supports reset of various parameters.
Parameters Description
Energy Resets the energy values. The meter supports reset of the following parameter values:
  • Active energy - Import / Export

  • Reactive energy - Import / Export

  • Apparent energy - Import / Export

  • Run Hour

DM Used for demand synchronization function. The meter supports reset of the following parameter values:
  • Last demand

  • Present demand

  • Predictive demand

Hi Lo Resets the minimum and maximum (min/max) values. The meter supports reset of the following parameter values:
  • V L-L average

  • V L-N average

  • Current average

  • Frequency

  • Active power, Total

  • Apparent power, Total

  • Reactive power, Total

  • Power factor, Total

MD Resets the maximum demand values.
  • W, VA, VAR, and current demand with timestamp

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.