NHA2779002-12

Example of over and under setpoint (standard) alarm operation

The meter supports over and under setpoint conditions on standard alarms.

A setpoint condition occurs when the magnitude of the signal being monitored crosses the limit specified by the pickup setpoint setting and stays within that limit for a minimum time specified by the pickup time delay setting.

The setpoint condition ends when the magnitude of the signal being monitored crosses the limit specified by dropout setpoint setting and stays within that limit for a minimum time specified by dropout time delay setting.

Over setpoint

When the value rises above the pickup setpoint setting and remains there long enough to satisfy the pickup time delay period (ΔT1), the alarm condition is set to ON. When the value falls below the dropout setpoint setting and remains there long enough to satisfy the dropout time delay period (ΔT2), the alarm condition is set to OFF.

The image represents alarm condition behavior over time, with a waveform transitioning through defined thresholds and delays. The y-axis includes setpoints A (pickup) and B (dropout), while the x-axis marks time progression with event indicators EV1 (start of alarm) and EV2 (end of alarm). Time intervals are labeled as ΔT1 for pickup delay, ΔT2 for dropout delay, and ΔT3 for total alarm duration. The diagram also highlights Max1 and Max2, representing the maximum values recorded during the pickup and alarm periods, respectively.
 

A

Pickup setpoint

 

B

Dropout setpoint

 

ΔT1

Pickup time delay period (in seconds)

 

EV1

Start of alarm condition

 

ΔT2

Dropout time delay (in seconds)

 

EV2

End of alarm condition

 

ΔT3

Alarm duration (in seconds)

 

Max1

Maximum value recorded during pickup period

 

Max2

Maximum value recorded during alarm period

     

The meter records the date and time when the alarm event starts (EV1) and when it ends (EV2). The meter also performs any task assigned to the event, such as operating a digital output. The meter also records maximum values (Max1, Max2) before, during or after the alarm period.

Under setpoint

When the value falls below the pickup setpoint setting and remains there long enough to satisfy the pickup time delay period (ΔT1), the alarm condition is set to ON. When the value rises above the dropout setpoint setting and remains there long enough to satisfy the dropout time delay period (ΔT2), the alarm condition is set to OFF.

The image represents alarm condition behavior over time, with a waveform transitioning through defined thresholds and delays. The y-axis includes setpoints A (pickup) and B (dropout), while the x-axis marks time progression with event indicators EV1 (start of alarm) and EV2 (end of alarm). Time intervals are labeled as ΔT1 for pickup delay, ΔT2 for dropout delay, and ΔT3 for total alarm duration. The diagram also highlights Min1 and Min2, representing the maximum values recorded during the pickup and alarm periods, respectively.
 

A

Pickup setpoint

 

B

Dropout setpoint

 

ΔT1

Pickup time delay period (in seconds)

 

EV1

Start of alarm condition

 

ΔT2

Dropout time delay (in seconds)

 

EV2

End of alarm condition

 

ΔT3

Alarm duration (in seconds)

 

Min1

Minimum value recorded during pickup period

 

Min2

Minimum value recorded during alarm period

     

The meter records the date and time when the alarm event starts (EV1) and when it ends (EV2). The meter also performs any task assigned to the event, such as operating a digital output. The meter also records minimum values (Min1, Min2) before, during or after the alarm period.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.