NHA2779002-12

Diag screens

The meter displays various diagnostics screens.
Screens Description
All LEDs on On entering diag screen, all LEDs on the front panel light up. The display shows four eights (8888), four decimal points (....) per line, negative indicators, and parameter LEDs. This indicates that the front panel LEDs and display are operating correctly.
Meter Model Displays the meter model number.
Serial number

Displays the meter serial number, for example SN.0500005174.

NOTE: Ensure you have your meter’s serial number information available while contacting Technical Support for help.

OS version Displays the operating system version number, for example OS 1.00.0.
RS version Displays the reset (boot code) version number, for example RS 1.00.0.
Diagnostics error code Displays the error codes of the meter for diagnostics.

For example: 0041 is the error code for Over-Running energy pulse output.

Run hours Delivered / Import Indicates the period the load has been delivered. This counter accumulates as long as the load is ON.
Received / Export Indicates the period the load has been received. This counter accumulates as long as the load is ON.
On hours Indicates the period for which the power meter's auxiliary supply is ON, regardless of the voltage and current inputs.
Interruptions Number of supply outages, means the number of auxiliary supply interruptions. If the power meter auxiliary supply is from a UPS then the INTR (number of interruptions) will be zero (as long as the UPS stays ON), even if the voltage signals die out from time to time.
RS-485 Communication error code Displays the communication errors of the meter.
Communication settings screen Displays the unit ID, baud rate, and parity values of the meter.
IO Displays the type of IO card used.
NOTE: Only PM2130 supports external IO cards. Other variants of PM2100 series meter do not support IO card.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.