NHA2779002-12

Display parameters

The meter displays various power system measurements.
Measurement Group Parameters Measured
System measurements Vavg, kVA, F, Iavg, kW, In, PFavg, kVAR, Iunb
Phase measurements VL-N, VL-L, I, kVA, kW, kVAR, PF, VTHD, ITHD
Demand measurements DM, PrsDM, PrdDM, MD
RTC / IO Date and time
NOTE: RTC is only applicable for meters with RS-485 communication. Meters with POP do not support this function.

The meter supports digital and analog IO.

NOTE: IO is supported only by PM2130 meter model. Other LED variants do not support IO function.
Energy readings

kWh (Active energy): Delivered / Received

kVAh (Apparent energy): Delivered / Received

kVARh (Reactive energy): Delivered / Received

NOTE: When the x 1000 LED is lit, multiply the displayed value by 1000 for the actual value.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.