NHA2779002-12

Button functions in viewing setup parameters

The meter supports single press and combination press functions of the buttons to view setup parameters.
Mode Button Function
Setup Menu To navigate to the next parameter configuration screen.
To navigate to the previous parameter configuration screen.
Enter setup mode to configure the displayed parameter value.
  

Press and hold the Up and Down buttons simultaneously for 2 seconds to enter Setup.

Exit setup with the same button sequence.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.