NHA2779002-12

Button functions

The meter supports single press and combination press functions of the buttons.
Symbol Description
To navigate down the list of items.
  Press and hold for 2 seconds. To move cursor to the left.
To navigate up the list of items.
  Press and hold for 2 seconds. To move cursor to the right.
To select a parameter.
  Press and hold for 2 seconds. To enter into or exit Clear page.

   

To enter into or exit Setup page.

 

To enter into or exit Diagnostics page.

   

To lock or unlock a meter page.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.