NHA2779002-12

Alarm priorities

Each alarm has a priority level that you can use to distinguish between events that require immediate action and those that do not require action.
Alarm priority Alarm display notification and recording method
Alarm LED Alarm logging
High Blinks while the alarm is active. Recorded in alarm log.
Medium Blinks while the alarm is active. Recorded in alarm log.
Low Blinks while the alarm is active. Recorded in alarm log.
None No activity Recorded in event log only.
NOTE: The alarm LED notification only occurs if the alarm / energy pulsing LED is configured for alarming.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.