NHA2779002-12

Button functions in viewing Diag screen

The meter supports single press and combination press functions of the buttons to view Diag screens.
Mode Button Function
Setup Menu To navigate to the next screen.
To navigate to the previous screen.
  

Press and hold the Down and OK buttons simultaneously for 2 seconds to view Diag.

Exit Diag screen with the same button sequence.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.