NHA2779002-12

Setting up the data log

You can select 2 items to record in the data log and the frequency (logging interval) that you want those values updated.

Use ION Setup to configure data logging.

NOTICE
Data Loss
Save the contents of the data log before configuring it.
Failure to follow these instructions can result in data loss.
  1. Start ION Setup and open your meter in setup screens mode (View > Setup Screens). See the ION Setup Help for instructions.
  2. Double-click Data Log #1.
  3. Set up the logging frequency and measurements/data to log.
  4. Click Send to save the changes to the meter.

    Parameter

    Values

    Description

    Status Enable, Disable Set this parameter to enable or disable data logging in the meter.
    Interval 15 minutes, 30 minutes, 60 minutes Select a time value to set the logging frequency.
    Channels Items available for logging can vary based on the meter type.

    Select an item to record from the “Available” column, then click the double-right arrow button to move the item to the “Selected” column.

    To remove an item, select it from the “Selected” column then click the double-left arrow button.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.