NHA2779002-12

Available standard alarms

Your meter has a set of standard alarms.
NOTE: Some alarms do not apply to all power system configurations. For example, line-to-neutral voltage alarms cannot be enabled on 3-phase delta systems. Some alarms use the system type and the VT or CT ratio to determine the maximum allowed setpoint.
Alarm label Valid range and resolution Units
ION Setup ION Setup
Over Phase Current 0.000 to 99999.000 A
Under Phase Current 0.000 to 99999.000 A
Over Voltage L-L 0.00 to 999999.00 V
Under Voltage L-L 0.00 to 999999.00 V
Over Voltage L-N 0.00 to 999999.00 V
Under Voltage L-N 0.00 to 999999.00 V
Over Active Power 0.0 to 9999999.0 kW
Over Reactive Power 0.0 to 9999999.0 kVAR
Over Apparent Power 0.0 to 9999999.0 kVA
Leading True PF -1.00 to -0.01 and 0.01 to 1.00
Lagging True PF -1.00 to -0.01 and 0.01 to 1.00
Over Frequency 0.000 to 99.000 Hz
Under Frequency 0.000 to 99.000 Hz
Over Voltage THD 0.000 to 99 %

Over Present Active Power Demand

0.0 to 9999999.0

kW

Over Last Active Power Demand

0.0 to 9999999.0

kW

Over Predicted Active Power Demand

0.0 to 9999999.0

kW

Over Present Reactive Power Demand

0.0 to 9999999.0

kVAR

Over Last Reactive Power Demand

0.0 to 9999999.0

kVAR

Over Predicted Reactive Power Demand

0.0 to 9999999.0

kVAR

Over Present Apparent Power Demand

0.0 to 9999999.0

kVA

Over Last Apparent Power Demand

0.0 to 9999999.0

kVA

Over Predicted Apparent Power Demand

0.0 to 9999999.0

kVA

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.