NHA2779002-12

Editing setup parameters

You can edit various measurement parameters as required.
  1. Press and hold the Up and Down buttons simultaneously for 2 seconds to enter Setup.
  2. Enter password. Default password is 0000.
  3. Press OK.
  4. Press the Up or Down button to select a parameter to edit.
    The selected parameter flashes the digit, value, or decimal point that is required to be set (the meter automatically determines which option to flash for editing, depending on the parameter).
  5. Increase or decrease the digit value, move the decimal point, or select a value from a pre-programmed list using the Up or Down button.
  6. Press OK after making the required changes.
  7. Press and hold the Up and Down buttons simultaneously for 2 seconds to exit Setup.
  8. Select Yes to save your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.