NHA2779002-12

IO LED Indicator

The IO LED indicator alerts or informs you of meters’ IO activities. The LED blinks at a constant pace when the IO module is attached to the meter.

A

IO LED indicator (Green)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.