NHA2779002-12

ION setup

Go to www.se.com and search for ION Setup to download a copy of the installation file.

If you already have an existing installation of ION Setup, it is recommended that you upgrade to the latest version in order to access new features or enhancements and properly configure features available on your device.

Refer to the online help to learn how to use ION Setup.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.