Create Fault
Available in ArcMap.
An operator can manually create a fault on a device or on a line (cut). A cut indicates a break in the line that disrupts power. Device incidents indicate a faulty device and can be placed on any devices that have the RXINCIDENTDEVICE model name assigned (see the Configuration Guide).
A fault can be created using this tool only on devices that are normally closed on any phase (e.g. NormalPosition = Closed). If you select a device that is normally open on all phases, you are prompted to use the Create Switching Operation tool instead. For example, if a customer calls and reports a transformer to be on fire, the operator can create an incident on that specific transformer.
Multi-Customer Loadpoints: When a fault is created on a multi-customer loadpoint (e.g. apartment building) using the Create Fault tool, all customers at the loadpoint are considered out.
- In ArcMap, locate the device or cut location on the map.
- Click the Create Fault
button on
the Responder toolbar.The cursor becomes a circle with a blue dot in the middle. The blue dot snaps to all selectable devices and lines. A layer must be set as selectable before this tool can snap to its features.
Placing a Cut: When placing a cut, you can press down the CTRL key to disable the snapping to devices. The cursor continues to snap to the line. This allows you to place a cut very near a device without snapping to the device. Cuts are always automatically confirmed when placed.
Origination: The Origination field allows you to manually create SCADA incidents. Any incident that has an Origination value of SCADA must also be confirmed. If you do not set the incident to confirmed, Responder issues a warning that the incident will be automatically confirmed.
- Click the faulty device or the cut location.
- The Create Incident dialog allows the operator to include
an outage time (unless the Cause is Non-Outage) and an estimated restoration
time.
The outage time must be the current time or earlier. Responder does not allow the user to provide a future outage time.
Non-Outage: If you select Non-Outage as the incident Cause, the Actual Status field equals the value in the Expected Status field. Once you click OK on the Create Incident window with the Cause set to Non-Outage, the Time of Outage field is set to null (since there was no actual outage).
Open Devices: If you place an incident on a device whose Expected Status is Open, the incident is automatically confirmed.
- Provide values in the editable fields on the Create Incident
window.In addition to the outage time you can modify the region, owner, confirmation status, hazard, remarks, etc. All fields in white can be edited. The Dispatcher field is filtered to display only the dispatchers that have access to the region in which the incident resides.
- Click OK.
Responder places an incident on the device or at the cut location. Responder's Prediction Engine identifies the affected upstream loadpoints and places outage symbology.
The outage area is highlighted on the map according to the symbology of the RxLineDisplay class. You must have this feature layer added to your map and the de-energized features functionality configured properly (see the Configuration Guide).
For incidents on normally open devices, the Actual Status defaults to the Phase Designation of the device. For all other devices, the Actual Status defaults to Open.