How to Mass Restore
- Select the devices you want to restore together.
- Right-click on one of the selected devices on the Incidents tab in Responder Explorer and select Mass Restore.
- Select a name in the Executed By drop-down. The selected name is applied to all devices selected for mass restore.
- Set the time of operation in the Time field. The set time
is applied to all devices selected for mass restore.TIP: Restore time must be later than the time of all outages.
- Add any remarks you have for the restoration in the Remarks box (this is not a required field). Those remarks are applied to all devices selected for mass restore.
- Click OK.
-
As with a single device restore, mass restore is only available for No Power outages.
-
Mass restore is only available if all the selected devices have not been restored.
-
If the restoration of a selected device is blocked by another feature (downstream ground, jumper causing phase swap), the restore process is halted until the blocking feature no longer blocks the restore.
-
If different crews are assigned to different devices to be restored, manual intervention is needed to choose a new crew member.
-
Mass restore is not available for devices on different incidents.