Edit Loadpoint
From the Edit Incident window, right-click a feature on the Affected Loadpoints tab and select Edit. The Affected Loadpoints tab displays all loadpoints associated with the incident. This includes features from any feature class with the FDRMGRLOADPOINT model name assigned (e.g., service points, transformers).
You can edit loadpoint information such as the number of customers impacted, time of operation, and restoration time. You cannot edit fields in gray. The Highlight, Zoom To, and Pan To tools are enabled only if you have ArcMap open.
You can delete a loadpoint, or multiple loadpoints (with permission), by right-clicking the selected loadpoints and selecting Delete.