Assigned Switching/Restoration Order
Use these steps if the switching or restoration order has been assigned to an incident. A template is never assigned to an incident.
- In Responder Explorer, expand the incident that has been assigned to the switching or restoration order.
- Right-click the switching or restoration order and select Edit.
- Use the Switching Order Editor to edit as needed.
- When you've finished editing the operations, click Save
from the Order menu and close the window.NOTE: If you click the red X in the window's upper-right corner, the entire window closes, along with any other switching orders in the window. If changes have been made to any switching order, a prompt appears for you to save the changes for each order.