View in ArcMap
Available in Responder Explorer.
Users can locate incidents, crews, tags, and incident devices on the map in ArcMap. Right-click an incident, crew, or incident device and select one of the following options:
-
Highlight: The feature (incident,
crew, tag, or device) flashes three times on the map. If the feature
is out of visible range, use the Zoom To tool before using Highlight. -
Zoom To: Changes the map display
so that the selected feature is visible. -
Zoom To Incident Extent: Changes
the map display so that the selected feature and its outage area are
visible. -
Pan To: Moves the map display
so that the selected feature is included without changing the map
scale. -
Quick Attribute Viewer: The Quick Attribute Viewer is a read-only display of feature attributes and values. Click the Quick Attribute Viewer to see attribute information about the fault device or feature.