Edit Crew Status/Time
Available in Responder Explorer.
After a crew has been assigned to an incident, you can change the crew's status on the Incidents tab using the Edit Crew Status/Time tool or the Change Crew Status tools. Edit Crew Status/Time allows you to select a status and edit the time that the crew changed to that status.
You can change the crew's status by right-clicking a crew in the Incidents tab or an incident in the Crews flyout window.
- Right-click a crew that has been assigned to an incident and select Edit Crew Status/Time. This displays the Time/Status Change window.
- The Status field displays the previous status, the current status, and the next logical status. Select a status from the drop-down menu.
- Set the time that the crew change was made. Click the Set
to Now
button to set the field to the current date and time.
- The updated crew status is reflected in the crew's Status field.