Move Fault Upstream
Available in Responder Explorer.
Move Fault Upstream lets the user change an unconfirmed electric device to the next upstream protective device. While the Change Device tool allows the user to select or search for any unconfirmed device in the map, Move Upstream automatically selects the next upstream protective device. The Move Fault Upstream tool is not available on confirmed fault devices.
A device can be moved upstream when it's downstream of another outage device; however, the moved device must be on a phase different than the upstream outage.
- Right-click an unconfirmed or probable fault device and
select Move Fault Upstream.The Edit Upstream Fault dialog displays information about the next upstream device.
- In the Status section of the dialog, edit the Actual, Time
of Operation, and Confirmed fields as needed.
The available values in the Actual field are determined by the device's Normal Status and Phase Designation. You cannot set an Actual Status of ABC on a device that has an expected status of A Closed and a Phase Designation of A. Responder adds this device to the incident in place of the selected device. The Confirmed status is automatically set to Probable, but you can edit the status as needed.
- Click OK to save changes and close the form.