Edit Tag

Available in ArcMap and Responder Explorer.

This tool allows you to modify information for existing tags. There are two ways to edit tags. You can select a tag to edit in either ArcMap or Responder Explorer.

  1. In ArcMap, click the Edit Tag button on the Responder toolbar.
  2. On the map, click a device that has a tag.
    The device must be selectable before this tool can snap to it.
  3. In Responder Explorer, right-click the tag on the Tags tab and select Edit.
  4. In the Edit Tag window in Responder Explorer, edit the Owner and Remarks fields as needed.
  5. Click OK to save your edits.

    If no tag exists on the selected device, the following message appears:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?