EVSOLCG001EN-01

Updating Network Settings

The Network screen is the following.

Update network settings (for example, IP, DNS) according to the information given by the IT manager of the customer site:

  • Device Name

  • EV Network:

    • Active DHCP client

    • IP Address

    • Subnet Mask

    • Default Gateway

  • DNS Server:

    • Preferred DNS Server

    • Alternate DNS Server

See IT plan and network information.

Factory settings are the following:

Fields Factory setting Description

Device Name

My EVCE device

Your EcoStruxure EV Charging Expert device

IP Address

192.168.0.128

Network IP address

Subnet Mask

255.255.255.0

Network sub-network mask

Default Gateway(1)

192.168.0.254

Gateway IP address. Mandatory to connect two networks so that devices on one network can communicate with the devices of another network.

Preferred DNS Server(2)

8.8.8.8

Preferred DNS server IP address(2)

Alternate DNS Server

Other DNS server IP address(2)

DHCP Server Configuration

OFF

ON/OFF

When DHCP server is managed by customer, DHCP server remains OFF.

(1) Address of the modem used for the connection to the supervision, if any. All charging stations are on the same sub-network as EcoStruxure EV Charging Expert and must be configured with the same gateway IP address.

(2) DNS server is used to convert URL to IP address. May be provided by the remote supervision (for example, through a dedicated SIM card). Google is the DNS server by default.

When you have finished updating network settings, select Save and Next.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.