EVSOLCG001EN-01

Other Products

For information about other products compatibility, recommendations and limitations, refer to:

Schneider Electric Power Meters

NOTE: Power metering is required when EcoStruxure EV Charging Expert is used in dynamic mode and to monitor photovoltaic production.

The following table lists the power meters from Schneider Electric that are compatible with EcoStruxure EV Charging Expert.

Refer to DOCA0358E EcoStruxure EV Charging Expert User Guide.

Name Pole description Input type Comment

A9MEM3250 (PAS600 + Acti 9 iEM3000)

3P / 3P + N

External current transformer (CT):1 A or 5 A

METSEPM5320 (PowerLogic PM5000)

3P / 3P + N

A9XMWD20 (PowerTag Link + PowerTag sensors)

3P / 3P + N

PowerTag wireless energy sensor up to 630 A

ComPact NSX circuit breaker with embedded metering (with Enerlin'X IFE gateway)

3P / 4P

Modbus TCP

For 3P, if you want to have power per phase with NSX 3-poles, you must add external neutral voltage tap.

MasterPacT MTZ circuit breaker with embedded metering (with embedded Enerlin'X EIFE module)

3P / 4P

Modbus TCP

For 3P, if you want to have power per phase with MTZ 3-poles, you must add external neutral voltage tap.

The following table shows the Modbus registers to get data, according to the type of power meter or circuit breaker.

  PM5320, IEM3x5x, PowerTag A ComPact NSX legacy ComPacT NSX MasterPacT MTZ

Register for current Ph1

3000

12016

32028

32028

Register for current Ph2

3002

12017

32030

32030

Register for current Ph3

3004

12018

32032

32032

Register for power Ph1

3054

12038

32077

32077

Register for power Ph2

3056

12039

32074

32074

Register for power Ph3

3058

12040

32076

32076

Register for total active power

3060

12041

32078

32078

Register for total active energy delivered

3204

12050

32096

32096

Other power meters that are not part of this selection are compatible with EcoStruxure EV Charging Expert as well.

When commissioning the power meter, select from the drop-down list on Model field, the corresponding model of power meter matching the appropriate registers list.

Modems

Use a 4G cellular modem (EVP3MM) with EcoStruxure EV Charging Expert. It is connected on the same network as EcoStruxure EV Charging Expert.

NOTE: Other modems with router function can be used.

Recommended Switches

Use Modicon Networking switch to integrate Ethernet solutions into your operation.

Unmanaged switch for star topology

Four ports for copper MCSESU053FN0

Eight ports for copper MCSESU083FN0

Managed switch for ring and daisy chain topologies

Four ports for copper MCSESM043F23F0

Eight ports for copper MCSESM083F23F0

For more information about communication network definition, refer to EVSOL1DG001EN eMobility Infrastructure Design Guide for Building Applications.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?