EVSOLCG001EN-01

If Installing EVlink Pro AC or Schneider Charge Pro

When internet connectivity is limited, install and configure AC charging stations one by one following the procedure that applies to the charging station range.

Procedures to Commission EVlink Pro AC

Follow one of these methods to update the EVlink Pro AC charging station firmware:

Procedure to Commission Schneider Charge Pro

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.