EVSOLCG001EN-01

Checking the Installed Firmware Version

  1. Check the installed firmware version for:

    • EcoStruxure EV Charging Expert

    • the charging stations (supported baseline)

    Use the latest release note of EcoStruxure EV Charging Expert and of the charging station that are available on se.com.

  2. If necessary, select Update Firmware to download the latest EcoStruxure EV Charging Expert firmware available from www.se.com.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?