EV Charging Station Ranges Compatible with EcoStruxure EV Charging Expert
The following sections indicate how to find support for commissioning each EV charging station range.
EV Charging Station Ranges Covered in this Guide
The following table indicates the characteristics of each EV charging station range covered in this guide.
| Charging station range | Power rate and phases availability | Minimum firmware version for compatibility with EV Charging Expert | Charging station commissioning |
|---|---|---|---|
EVlink Pro AC![]() |
From 7.1 kW to 22 kW 1P or 3P |
1.3.8 |
See Procedure to Update EVlink Pro AC Charging Station Firmware. Refer to the video showing how to commission EVlink Pro AC charging station with eSetup: |
|
From 7.4 kW to 22 kW 1P or 3P |
1.18.1 |
See Updating EVlink Schneider Charge Pro Charging Station Firmware. Refer to the video
showing how to configure Schneider Charge Pro with eSetup: |
Other EV Charging Station Ranges not Covered in this Guide
-
EVlink Smart Wallbox (legacy range)
-
EVlink Parking (legacy range)
-
EVlink Pro DC 60 kW
-
EVlink Pro DC 60 V2
-
Schneider StarCharge Fast 60 kW
-
EVlink Pro DC 180 kW
-
EVlink Pro DC 180 V2
-
Schneider StarCharge Fast 180 kW
-
EVlink Pro DC 320 kW
-
Schneider StarCharge Fast 320 kW
For EV charging station ranges not covered in this guide, contact your local Schneider Electric front office.