EVSOLCG001EN-01

Before You Begin

Electrical monitoring and control equipment, and related software are used in a variety of buildings. The type or model of electrical monitoring and control equipment suitable for each application varies, depending on factors such as the system dependability level, unusual conditions and government regulations.

Only the user can be aware of all the conditions and factors present during setup, operation, and maintenance of the solution. Therefore, only the user can determine the electrical monitoring and control equipment and the related safeties and interlocks which can be appropriately used. When selecting electrical monitoring and control equipment, and related software for a particular application, the user should refer to the applicable local and national standards and regulations. The National Safety Council's Accident Prevention Manual (nationally recognized in the United States of America) also provides much useful information.

Ensure that appropriate safeties and mechanical/electrical interlocks protection have been installed and are operational before placing the equipment into service. All mechanical/electrical interlocks and safeties must be coordinated with the related automation equipment and software programming.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?