EVSOLCG001EN-01

Using eSetup to Enable RSTP on EVlink Pro AC Charging Stations

The firmware version installed on EVlink Pro AC charging stations is at least 1.3.8.

The eSetup application version is at least 13.1.3.

Otherwise, when configuring a ring topology, a pop-up window appears on the application and asks you to update the Pro AC firmware to proceed with its configuration.

Refer to the documentation for updating the EVlink Pro AC charging stations: EVlink Pro AC – Professionals.

For more information about how to configure Ethernet communication parameters with eSetup, refer to the video showing RSTP activation for a ring topology.https://www.youtube.com/watch?v=Sg7sAeqko_w&t=89s

To configure charging stations with eSetup:

  1. Check the installation.

  2. Enable RSTP.

To activate the RSTP protocol, click Activate RSTP > ON.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?