EVSOLCG001EN-01

Assigning Charging Stations

To assign charging stations to a zone according to the electrical distribution plan and to the defined EVSE architecture:

  1. Select the installation wizard.

  2. In the Stations Assignment menu, in the Unassigned Stations list, select the charging station you want to assign to a zone.

  3. Move Selection To a created zone.

    The Unassigned Stations list is automatically updated.
  4. When you have assigned all charging stations to a zone, select Save and Finish.

For more information about the assignment of charging stations to a zone, refer to the video showing how to configure loads' parameters with EcoStruxure EV Charging Expert & assign chargers to a zone:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?